Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

25 kW High Efficiency High Power Density Bi-directional T-type Inverter [CRD-25BDA6512N-K] Gerbers

Tiago
Tiago Contributor Level 1
edited September 2024 in General

Hi,

In the main page for CRD-25BDA6512N-K links for PCB do not have GERBERs files. Can you please provide them?

Also, the main coils ( L5_1, L5_2, L5_3) are not specified on the BOM. Neither is the specficiation for them. Can someone please help us with this?

For grid tied, are there any news regarding the possibility to use in this working mode? This is very important for us.

Best regards,

Tiago Borges

This discussion has been closed.