Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

sixpack module gate voltage and junction temperature measurement

sayed
sayed Contributor Level 1
edited October 2024 in Module Products

HI ,

i am using CCB021M12FM3 six pack module to design inverter with PMSM load as you can see in the attachment. i have some question on its results.

1 it shows gate voltage of around 0-700V when i have given a voltage of around -4-16V. why its shows 700v in the circuit

2. the junction temperature of the circuit is also very high and it is in KV , why the temperature reading is in Volts . how to get this voltage reading in Kelvin or Celsius.

3 why the input current to the inverter shows negative

This discussion has been closed.