Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Over current Protection in CRD25DA12N-FMC

GayanvDissanayake
GayanvDissanayake Contributor Level 1
edited February 2025 in General

"Hi! Could you please clarify whether the overcurrent protection in the 25kW SiC Wolfspeed Converter (CRD25DA12N-FMC) is implemented as a built-in tripping mechanism or through your CCS code?"

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5

    Hello,

    The CRD25DA12N-FMC does not include a built-in overcurrent tripping mechanism. The trip can be configured in CCS code by using the high/low limit of the Post Processing Blocks (PPBs) feature of the controller analog-to-digital converters (ADCs). The PPBs can be used to monitor if the current measurement exceeds a pre-defined value. Alternatively, the "Overcurrent References" resistor dividers on the schematic can be adjusted to a pre-defined trip voltage which equates to a relevant current. An interrupt can be configured in the controller to trigger when one of the overcurrent detection operational amplifier circuits is tripped.

    Thanks,

    Chris N.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.