Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Dies in modules

Options
FMPower
FMPower Contributor Level 1
edited February 20 in Module Products

Can you confirm that all 6 devices in the CCB016M12GM3 have separate dies or do any devices share dies? The concern being the potential of latchup that may occur when multiple devices share a die.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4
    Options

    There are 6 independent switch positions in the CCB016M12GM3. The die are not shared between the positions and there is not a concern of latch up.

    Best Regards,

    Austin C.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. If it did, please click on "This question has been answered - Close Discussion" . If you have a follow up question, at a later date, please "Start a New Discussion"

This discussion has been closed.