Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Aluminum Nitride Thermal Interface Material

PEwithQuestions
PEwithQuestions Contributor Level 1
edited February 2025 in General

Hi,

For the Aluminum Nitride thermal interface material 32mmx32mmx1mm, how much pressure is supposed to be applied to the AlN sheet? Is there a pressed ratio (like 1mm thickness should be pressed to 0.9mm)? This material is stiff and brittle, maybe there shouldn't be much pressure applied to it and it's not supposed to be pressed down and shrink?

Thanks.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • BGochis
    BGochis Wolfspeed Employee - Contributor Level 2

    Hello,

    AlN TIM material does not need a pressure applied to it specifically to enable it's thermal properties (such as other TIMs like Sil-Pads require). The only pressure that it needed is the mounting pressure used to attach the discrete package itself by screw, clip, or any other mounting configuration used into the system. This will help limit the contact resistance between the package and AlN (recommend to use thermal grease as well). Any additional pressure will risk damaging the AlN as it is a very brittle material and could lead to cracking and loss of electrical isolation while not providing any additional thermal benefits

    Thanks

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. If it did, please click on "This question has been answered - Close Discussion" . If you have a follow up question, at a later date, please "Start a New Discussion"

This discussion has been closed.