Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD25DA12N-FMC as a three phase power supply

Options
Andras_Magyar
Andras_Magyar Contributor Level 1
edited March 2025 in General

Dear Experts,

I would like to use CRD25DA12N-FMC as a three phase DC to AC power supply up to 10kW max.

My questions are:

  • Do you have a firmware that support off-grid mode of this power supply maybe with active power control?
  • In the PCB there is no null output just the three phases. How can we achieve that?

Thanks and regards,

Andras Magyar

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Andras_Magyar
    Andras_Magyar Contributor Level 1
    Options

    Thank you very much in advance!

  • ChrisN
    ChrisN Wolfspeed Employee - Contributor Level 4
    Options

    Hello Andras,

    Thank you for your interest in this product. We have firmware that supports sine pulse width modulation (SPWM) open-loop control. This firmware can be modified to fit the end application needs. The firmware is available for download from the webpage for this design. Regarding the null, this design has been tested with line-to-neutral loads with a floating neutral, so a null connection was not necessary on the board.

    Thanks,
    Chris N.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.