Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD25DA12N as an off grid inverter

Options
Andras_Magyar
Andras_Magyar Contributor Level 1
edited March 2025 in Module Products

Dear Experts,

We would like to use CRD25DA12N as an off-grid three phase power supply for railway applications and this module would be perfect for quick evaluation. The only problem is that we do not have code that can work in a closed loop system regulation for standard European three phase output 400Vac/50Hz.

So the requirements we need:

Vindc= 500Vdc

Vout=400Vac

Line frequency = 50 Hz

Poutmax = 8kW

Also we need the N neutral which we think can be the middle point between +/-DC input voltage. Is it right?

Could you please provide some help how to get this software for this module?

We have some TI resource for the control theory, link here (starting from page 32):

https://www.ti.com/lit/ug/tidue53i/tidue53i.pdf?ts=1739817665967&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FTIDA-01606

We do not want to get into the details because it can be complicated only that it would work autonomously regulation voltage, current or whatever best fit for the application.

Thanks and regards,

Andras Magyar
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
    Hello Andras,

    CRD-25BDA6512N-K is optimized for Vin= 650V-900VDC and doesn't work very well below 650VDC input for 400Vac output voltage. However since your power is also limited 8kW, you can play around with the firmware to optimize it for those conditions.

    You can also use our https://www.wolfspeed.com/tools-and-support/power/speedfit/ to choose the correct devices for your system conditions and topology.

    If you need a neutral connection, you can use the connection below to connect a neutral wire. However the design and firmware have not been tested with a neutral connection.

    Have you filled out firmware request for on this page?

    https://www.wolfspeed.com/products/power/reference-designs/crd-25bda6512n-k/

  • Andras_Magyar
    Andras_Magyar Contributor Level 1
    Options

    Hi,

    Yes I have filled out the request for the firmware but I have not got it yet.

    Can you provide it?

    Thanks,

    Andras

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hello Andras,

    We're having a temporary issue with sharing the firmware files through our system. I expect it to be fixed in a few days, will send you the firmware as soon as it is resolved. Thank you for your patience.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hello Andras,

    The firmware files have been sent to your registered email id. Let me know if you need anything else. Thank you!

This discussion has been closed.