Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD300DA12E-XM3: How to increase the 500Hz fundamental frequency limit of the GUI.

Options
Pete
Pete Contributor Level 1
edited February 2025 in Module Products

Hi there,

We purchased a CRD300DA12E-XM3 and set up the controller with the Wolfseed's default GUI.

In the GUI, we found that the upper limit of the fundamental frequency is preset to 500Hz. Is there any way to increase this limit in the GUI? Are there any hardware limits that prevent us to do so?

Thanks in advance!
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
    Hi Pete,

    The fundamental frequency limit of 500 Hz on the CRD300DA12E-XM3 actually comes from a United States export controls limitation. You are free to edit the firmware to exceed this rating and the hardware can support it; the user guide contains all of the information necessary to install TI's Code Composer Studio to make changes to the DSP's firmware.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Pete
This discussion has been closed.