1200VSIC的驱动器与1700SIC驱动器选择
如果使用模块化的1200V的SIC功率器件(CAB011M12FM3,CCB032M12FM3),驱动器采用CGD1700HB2M-UNA配合差分CGD12HB00D可以驱动吗?如果使用分立的SIC(C3M0021120K)器件,可以使用上述的驱动器进行驱动吗?
对于1700V的SIC器件,有没有配套的SIC型号(模块化与分立的都可以)以及对应的驱动板?CGD1700HB2M-UNA配合差分CGD12HB00D可以驱动1700V的SIC吗?如果可以,说一下SIC的型号(模块化与分立的都可以)
Comments
-
Hello, thank you for your message. A member of our technical team is looking into your questions and we will respond shortly.
0 -
可以帮忙配置出耐压值1200V,电流大于15A最合适的SIC型号(模块化与分立的都可以)以及驱动器型号吗?也可以提供选择的
可以帮忙配置出耐压值1700V,电流大于15A最合适的SIC型号(模块化与分立的都可以)以及驱动器型号吗?也可以提供选择的
0 -
To correctly understand the question:
"If a modular 1200V SIC power device (CAB011M12FM3, CCB032M12FM3) is used, can the driver be driven by CGD1700HB2M-UNA and differential CGD12HB00D? If I use a discrete SIC (C3M0021120K) device, can I use the above driver for driving?
For the 1700V SIC device, is there a matching SIC model (both modular and discrete) and the corresponding driver board? Can CGD1700HB2M-UNA and differential CGD12HB00D drive 1700V SIC? If possible, please tell me the model of the SIC (both modular and discrete)
Can you help to configure the most suitable SIC model (both modular and discrete) and driver model with a withstand voltage of 1200V and a current greater than 15A? Optional
Can you help me configure the most suitable SIC model (both modular and discrete) and driver model with a withstand voltage of 1700V and a current greater than 15A? Optional"
Is that correct?
0 -
Hello Light,
Yes, the CGD1700HB2M-UNA paired with the CGD12HB00D can drive a 1,200 V FM3 WolfPACK power module or a 1,200 V discrete device such as the C3M0021120K.
Yes, the CGD1700HB2M-UNA paired with the CGD12HB00D can drive a 1,700 V power module or discrete. To provide an example, the CAB320M17XM3 power module could be driven with this driver.
If you're looking for a gate driver with a peak output current of 15 A, you may need to design your own board. There are many driver ICs capable of hitting this peak current such as the Texas Instruments' UCC5870 or UCC5880 or IXYS's IXD_630 or Analog Devices' ADuM4177. Wolfspeed's CGD1700HB3P-HM3 gate driver is capable of peak currents up to 14 A with a 1,700 V working voltage capability, which may meet your application's needs.
Best Regards,
Austin C.
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0