CRD200DA12E-XM3
I have following queries regarding CRD200DA12E-XM3
- What is the operation environment (temperature)?
- Is CAN interface is mandatory? Or we can Bypass the CAN interface and only work with the DSP Launchpad?
- Can we change the source code from CAN interface?
- Can we change the source code from the DSP Lauchpad?
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello,
Any update on this?
0 -
Hi aa2719,
The inverter was designed to operate in a lab environment with the temperature around 25°C, but it is possible to operate at higher ambient temperatures. The ripple current on the capacitors and the power draw on the gate drivers due to the switching frequency will play a role in determining your maximum allowable ambient operating temperature. Did you have a particular target ambient temperature?
You are not required to use the CAN interface, but it greatly simplifies the testing of the unit. You can bypass the CAN interface and work only with the DSP Launchpad.
You are free to make any changes to the inverter reference design as desired. You can change the source code by requesting the firmware on the landing page for the CRD200DA12E-XM3.
Best Regards,
Austin C.
0 -
Thanks for the reply.
Can you answer also the below queries?
What will be the best procedure to bypass the CAN?
Can I bypass it through the source code? or I need to do it physically?
aa2719
0 -
Hello All,
Can you answer also the below queries?
What will be the best procedure to bypass the CAN?
Can I bypass it through the source code? or I need to do it physically?
aa2719
0 -
Any comment on above?
0 -
Hi aa2719,
I would recommend that you bypass the CAN in the source code. If you handle the software correctly, there shouldn't be anything that needs to be changed physically on the board to bypass CAN.
Best Regards,
Austin C.
0 -
I have requested the firmware from the landing page but did not receive any. If you can escalate it, that would be helpful.
0 -
Hi aa2719,
The firmware was already sent. I would like to confirm you received it.
Thanks,
0 -
I have received it
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0