internal gate resistance
Hello,
In the datasheet of the HM3 and XM3 SiC power modules, the internal gate resistor's value is given. I want to ask is the internal gate resistance given in the power module datasheet the MOSFET's intrinsic RG, or it is the value of the gate resistor integrated inside the power module?
For the CAS480M12HM3, the RG(int) is given and the test condition is also given of 100KHz. So is this RG(int) is the MOSFET's gate resistance?
While for CAS480M12HM3, the RG(int) is given but no test condition is given. Is this the integrated gate resistor's value?
Thanks!
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
WWB,
The internal gate resistance given in the module datasheet is the total gate resistance as seen from outside of the module. The test conditions are 25 mV, 100 kHz.
Thanks,
Paul Kanatzar
0 -
Hi Paul,
I see. Thanks for your reply.
WWB
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0