Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

How to properly connect Tj and Tc for LTspice simulation of C6D10170H

LeoLuchetti
LeoLuchetti Contributor Level 1
edited August 2023 in Discrete Products

Hello, with other SiC Part models the Tj and or Tc pins need to be connected to a voltage source in order for the device to behave properly. How should the Temperature pins be connected for the model of C6D10170H?

I currently have just Pin 2 (anode) and the case (Cathode) connected to the circuit.

Thanks,

Leo

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ZMiller
    ZMiller Wolfspeed Employee - Contributor Level 3

    Hi Leo,

    You can connect a voltage source directly to Tj if you want to fix the junction temperature during the simulation. If you connect the voltage source to Tc, you can fix the case temperature for the simulation and probe the Tj node (you'll need to extend a wire from the connection point) to see how the junction is changing with a fixed case temperature. If you add a resistor between Tc and this voltage source, you can model ambient temperature with the voltage source and have a variable case and junction temperature for the simulation.

    I hope that helps.

    Thanks,

    Zack

  • LeoLuchetti
    LeoLuchetti Contributor Level 1

    Can you have multiple devices Tj or Tc pins connected to the same voltage source or do they need to be connected to independent voltage sources?


    What affect does it have on the simulation if you leave the Tj and Tc pins disconnected?


    Thanks

  • ZMiller
    ZMiller Wolfspeed Employee - Contributor Level 3

    Hi,

    You can connect them to the same source, that isn't an issue. I'd recommend attaching the Tj pin for each device to the same voltage source when fixing the junction temperature. If you're attaching them all to the case, add a series resistor between the voltage source and the Tc pin to model Rch. You should attach at least one pin, otherwise the simulation may fail.

    I hope this helps!

    Thanks,

    Zack

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.