Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD25DA12N-FMC power loop inductance

Options
jiten000
jiten000 Contributor Level 1
edited August 2023 in Module Products

Hi, there are only 3 x 65 uF capacitors are present and no high frequency capacitors are used in the DC-Link of this design. DC+ and DC- is interleaved across 4 layers. Can you share the power loop inductance of this design?
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
    Hello jiten000,

    Thank you for your question. The power loop inductance was measured to be 8.6 nH at 10 MHz. The measurement results are provided below. 


    Thanks,

    Chris N.

  • jiten000
    jiten000 Contributor Level 1
    Options

    Hi Chris,

    Thanks for your reply. What is the overshoot observed on Drain?

    Regards,

    Jitendra

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 4
    Options

    Hello Jitendra,

    Thank you for your follow-up question. Below is a oscilloscope screenshot from one of our experimental tests. The maximum observed VDS in our testing was 1.03 kV (230 V of overshoot on 800 V bus), which is well within the safe operating region of the power module. The operating conditions for this experiment are summarized in the table below. If necessary, this overshoot can be reduced by increasing the gate resistances. 

    Thanks,

    Chris N.

  • jiten000
    jiten000 Contributor Level 1
    Options

    Thanks

This discussion has been closed.