Dynamic thermal parameter for CAB006M12GM3
Hi Sir,
can we provide foster fourth-order thermal parameters of CAB006M12GM3 for customer, like below, thanks
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hi Wei,
Here are the parameters for a 3rd-order Foster network following the format below. This should be sufficient for the customer (I am having a small issue with the 4th-order). If they have to have a fourth order circuit, let me know and I'll get it fixed.
R1 = 0.20759, R2 = 0.0028637, R3 = 0.022834
C1 = 0.27484, C2 = 0.0012515, C3 = 0.033355
Here is a comparison between the CAB006M12GM3 Zth data and the 3rd order fit for the above parameters.
Thanks,
Brian
0 -
I was able to figure it out. Here is the 4th order.
R1 = 0.0018372, R2 = 0.031065, R3 = 0.0082913, R4 = 0.19263
C1 = 0.00084193, C2 = 0.12324, C3 = 0.016418, C4 = 0.35435
0 -
Hi Tangwei,
I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
Blake
0 -
thanks for great support!
0