Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Simetrix compatability issues

MSW
MSW Contributor Level 1
edited March 2024 in Discrete Products

Hi,

this SiC "E3M0016120K" spice model is working perfectly in LTspice, but I am getting this following error, when i try to run it in simetrix.

image.png

Can you please help in fixing this error

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • sparasaram
    sparasaram Wolfspeed Employee - Contributor Level 1

    Hi MSW,

    Running the latest available E3M0016120Kmodel from Wolfspeed website, I was not able to recreate the issue.

    I'm showcasing a simulation implementing a simple circuit shown below. I didn't see the issue mentioned by you.

    This might be a version issue of SIMetrix (I'm currently using 9.10m (x64) version). If possible can you also send the .lib file you are having this issue with?

    Thank you,

    Sparasaram

    image.png
  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. If it did, please click on "This question has been answered - Close Discussion" . If you have a follow up question, at a later date, please "Start a New Discussion"

This discussion has been closed.