Speedval kit optimum PWM frequency
We have the speedvalkit platform with following configs
- MOD-PWR-MM-C3M0032120K
- 400uH Buck / Boost filter board
We plan to test a buck converter config from 800V to 400V DC. What is the desired PWM frequency the 400uH inductor has been optimized for peak efficiency . Our load is 12A current.
Comments
- 
            Thank you for your post, it has been approved and we will respond as soon as possible. 0
- 
            Hello mavern1, The SpeedVal kit buck/boost boards are designed for general purpose evaluation. They were not optimized for a particular operating point or tested to identify the peak efficiency as a function of frequency. To find the frequency for peak efficiency, you will have to take some frequency vs efficiency measurements. Recommended frequency range is 20 to 100 kHz. I recommend referring to the synchronous "boost" application example in the SpeedVal Kit Half-Bridge Motherboard User Guide. 66 kHz is used for testing in that example. A few other guidelines on synchronous buck configuration are highlighted in Section 8.3 of the user guide. I hope this helps. Thanks! Urvi 0
- 
            Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further. 0