Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Issues during turn off of SiC MOSFET C3M0120090D in Asymmetrical Half-Bridge converter

Options
Kalpak
Kalpak Contributor Level 1
edited May 2024 in Discrete Products

Hello,

I am trying to make Asymmetrical Half-bridge converter using two SiC MOSFETs(C3M0120090D) and two diodes. I am getting ambiguous waveform of drain-source voltage, load current and load voltage during turn-off period. During turn-off, load current is getting higher and then settling to zero. There is overshoot in Vds also. I am not able to understand why this kind of waveform is coming.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hello Kalpak,

    Are the 2 SiC MOSFET C3M0120090D in parallel? Which topology is the converter? Which diodes are you using? What is the switching frequency? Thank you so much!

  • Kalpak
    Kalpak Contributor Level 1
    Options

    Yes, the 2 SiC MOSFETs are in parallel. I am using two ultra-fast Si diodes (MUR1560) and my switching frequency ranges from 5kHz to 50kHz. The above-shown results are for 5kHz switching frequency. I am using Asymmetrical Half-bridge topology as shown below.

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 3
    Options

    Greetings Kalpak:

    I am looking at the waveforms in the first image and have a question. It shows only one gate (Vgs) high at a time. Looking at your schematic, how can you get current to begin flowing without gating both switches? If there was current already flowing through the inductor, one could turn on just one gate and the current would freewheel through one of the diodes but here the current is starting from zero.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. If it did, please click on "This question has been answered - Close Discussion" . If you have a follow up question, at a later date, please "Start a New Discussion"

This discussion has been closed.