Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Bare die soldering

Yang
Yang Contributor Level 1
edited May 2024 in Bare Die Products

Hi,

I am a student from University of Tennessee, Knoxville. Recently, I am trying to test a bare die. However, I find myself in trouble with the soldering of the SiC dies. The finish of source and gate pads are aluminum, which is hard for me to solder in lab. Do you guys have some ideas on how to solder them?

Thanks,
Yang

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • DHofmann
    DHofmann Wolfspeed Employee - Contributor Level 2

    Hi Yang,

    what kind of trouble do you face?

    Bare dies are not supposed to soldered by hand. Common source attaches are bond wires or clips.

    In case of manual hand soldering, there is a high risk of damaging the die.

    However, you may use a solder material that is available in a preform. Then solder a metal clip on top.

  • Yang
    Yang Contributor Level 1

    Hi,

    Thanks for your kind response. The finish of source and gate pads are Al, which cannot be soldered. Do you provide bare dies with other finishes on gate and source pads?

    What is solder material available in a perform? Could you explain more about this? Thanks!

  • DHofmann
    DHofmann Wolfspeed Employee - Contributor Level 2

    Hi,

    suggested alloy for aluminum alloy soldering is 91/9 tin. Zinc bonds with aluminum. Another common alloy suggested for aluminum is 96.5/3.5 tin.

    For an electrical contact, its works.

  • Yang
    Yang Contributor Level 1

    Hi,

    These soldering is used with extra flux, which is usually acid. Would the acid damage the bare die, as the finish of aluminum is pretty thin.

    Additionally, could you help me check whether Wolfspeed provide customized bare dies with other finishes on gate and source pads?

    Thanks

  • DHofmann
    DHofmann Wolfspeed Employee - Contributor Level 2

    I consider that you do not need reliability since you manually process the die. Therefore, the flux material does not damage the die for your test purposes.

    We do not offer a customized finish for manual hand soldering.

    Would you mind providing more information on what you need to do?

    We can also take the conversation offline.

  • Yang
    Yang Contributor Level 1

    Hi,

    I want to design and fabricate a power module in the lab. Can you provide your email? We can communicate with emails.

  • DHofmann
    DHofmann Wolfspeed Employee - Contributor Level 2

    Let me contact you to continue the discussion

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.