Gate Drivers disabled with HVDC in CRD300DA12E-XM3
Hi there,
I'm wondering if the gate drivers shall be powered-up (PSDIS signal from the LaunchPad) before high voltage is set in the DC side.
I've faced in the past issues with IGBTs if the gate drivers are not power-up and there is high voltage is the DC side.
Best regards,
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello BorjaH,
It is best practice to enable power to the gate drivers before applying high voltage to the DC bus.
The modules will block voltage at VGS = 0 V, but it is safest to ensure that the drivers are providing VGS = -4 V before introducing a bus voltage. We have also included VGS bleeder resistors on the gate driver boards to prevent charge-up of the gate to help ensure the modules block voltage in a power supply disabled state.
Best Regards,
Austin C.
0 -
Hi Austin,
Thank you very much for your feedback.
All is clear now!
Borja
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0