C6D08065Q - Can you connect the N/C pins on the QFN package to a polygon to aid in heat dissipation?
Hello. I am working on a passive rectifier PCB design using the C6D08065Q SiC diodes and I am wondering if connecting the N/C pins to a polygon would cause issues with the performance of the device. I am thinking that it would be beneficial to connect them to a large copper surface to help with heat dissipation. In addition, would it be safe to assume the same thermal management process as a SiC MOSFET in a similar package (vias to reverse of PCB then heatsink)? Thanks.
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Thanks for your interest in our SiC diodes. Regarding your question, there shouldn't be a concern from the device standpoint, but connecting NC pins to a polygon/copper pad will not provide a noticeable improvement to heat dissipation since most of the heat goes directly down from the die into the PCB. Hope this helps.
0 -
Sounds good, that makes sense. Thank you for your help.
0 -
You're welcome! We have an App Note on SM device thermal management. Please take a look. Hope it can be of some help.
Here is the link.
0