Request About Temperature of TOLL information confirmation
Dear Support team,
Could you help us to confirm below tempature information which are right? If the values are all correct in our datasheet, why 25mhom have different Tc&Tstg values compare others?
Tc | Tstg | Tj | |
|---|---|---|---|
C3M0025065L | 175 | 175 | 175 |
C3M0045065L | 150 | 150 | 175 |
C3M0060065L | 150 | 150 | 175 |
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Wen,
The table you have shown is correct. The reason that the 25mohm is rated to 175C Tc and Tstg is due to the fact that it was released later than the rest of the portfolio and had additional pre-mold plasma clean and therefore was tested to a wider temperature range. There is work ongoing to match the rest of the portfolio to the 175C temperature that the 25mohm has but as of now the testing has not been done to prove this capability
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0