Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Change the driver board parameters

Options
Emma
Emma Contributor Level 2
edited December 2024 in Module Products

Hello, I met some difficulties when selecting the type of drive board. I want to drive the CAS480M12HM3 half-bridge module, and I chose CGD1700HB3P-HM3, but I still need to change the drive voltage and drive resistance on the drive board to explore the influence of the drive loop parameters on the switching characteristics. How can I change the driving voltage and driving resistance?

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • PaulKanatzar
    PaulKanatzar Wolfspeed Employee - Contributor Level 2
    Options

    Emma,

    The design files for the CGD1700HB3P-HM3 can be downloaded here. The negative drive voltage can be adjusted with the linear regulators (UT10 and UB1) by adjusting RB9 and RT20.

    The turn on and turn off gate drive resistors (RT2, RT3, RT27, RT28) can be changed to adjust the gate drive resistance after removing the heatsink.

    Adjustment of the positive drive voltage is not easily achievable.

    -Paul

  • Emma
    Emma Contributor Level 2
    Options

    Thank you for your answer. But I need to study the effect of drive voltage on SiC MOSFET loss. How can I change the positive drive voltage?
    Looking forward to your reply, thank you

  • PaulKanatzar
    PaulKanatzar Wolfspeed Employee - Contributor Level 2
    Options

    Emma,

    It is not designed to adjust the positive voltage rail. Additional circuitry is required to regulate the voltage down. The CGD1700HB2P-BM3 has the pads for a LDO to tune the gate drive voltage. If you have Altium you could change the pin headers in the design and use that driver instead?

    There is not an easy solution currently available.

    Thanks,

    -Paul

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.