C3M0025065J1 what is the max. IDSS for 350V and 75°C
Hello,
I'm dealing with the C3M0025065J1 sic-Mosfet.
The working contions are @75°C and 350V Uds.
I would need more exact data for the max Idss (zero gate voltage drain current) for ~75°C and ~350V. Are this data availbale?
many thanks
Alex
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
We'll get back to you shortly
0 -
Thanks for your question.
From the datasheet, maximum Idss at 650 V/25 °C is 50 µA. Using a voltage scaling factor of 350 V/650 V = 0.54 and temperature scaling factor of 75°C/25°C = 3, you will get 81 µA approximately for Idss at 350 V/75°C. You can use 100 µA maximum for conservative design.
Hope this answer your question.
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0