CRD25DA12N as an off grid inverter

Dear Experts,
We would like to use CRD25DA12N as an off-grid three phase power supply for railway applications and this module would be perfect for quick evaluation. The only problem is that we do not have code that can work in a closed loop system regulation for standard European three phase output 400Vac/50Hz.
So the requirements we need:
Vindc= 500Vdc
Vout=400Vac
Line frequency = 50 Hz
Poutmax = 8kW
Also we need the N neutral which we think can be the middle point between +/-DC input voltage. Is it right?
Could you please provide some help how to get this software for this module?
We have some TI resource for the control theory, link here (starting from page 32):
We do not want to get into the details because it can be complicated only that it would work autonomously regulation voltage, current or whatever best fit for the application.
Thanks and regards,
Andras Magyar
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello Andras,
CRD-25BDA6512N-K is optimized for Vin= 650V-900VDC and doesn't work very well below 650VDC input for 400Vac output voltage. However since your power is also limited 8kW, you can play around with the firmware to optimize it for those conditions.
You can also use our
to choose the correct devices for your system conditions and topology.If you need a neutral connection, you can use the connection below to connect a neutral wire. However the design and firmware have not been tested with a neutral connection.
Have you filled out firmware request for on this page?
0 -
Hi,
Yes I have filled out the request for the firmware but I have not got it yet.
Can you provide it?
Thanks,
Andras
0 -
Hello Andras,
We're having a temporary issue with sharing the firmware files through our system. I expect it to be fixed in a few days, will send you the firmware as soon as it is resolved. Thank you for your patience.
0 -
Hello Andras,
The firmware files have been sent to your registered email id. Let me know if you need anything else. Thank you!
0