Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Max Dvdt for 1200V 40mR TO247-4 Device

Options
David2023
David2023 Contributor Level 1
edited July 1 in Discrete Products

I want to know the max dvdt for C3M0040120K ? 100V/ns ? Thanks.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Yes that is correct. You can also refer to this post. Thank you!

  • David2023
    David2023 Contributor Level 1
    Options

    Thanks Tbhatia.

    I find that infineon's datasheet (IMW65R060M2H)shows the max dv/dt is 200V/ns.

    Could you please help double check the maximum dV/dt rating of C3M ? Thanks a lot!

    Best regards

    David

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hello David2023,

    100V/ns is generally plenty for most applications. Are you just comparing specifications or do you really wish to switch that fast? Thanks!

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hello David2023,

    Any update on your dv/dt requirements?

    Thanks!

This discussion has been closed.