Suitable power device for 208VAC, 480VAC, 40A AC switching application
Application : We are developing a AC switching circuit using dual MOSFET configuration. The application is for driving the 208VAC, 480VAC, 40A AC heaters to control its temperature.
1. Is it preferred to use MOSFET or IGBT for this?
2. Which MOSFET series is preferred for this application?
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello meghanam,
It depends. I'd like to ask you couple of more questions about your topology:
- Is this a soft-switching topology?
- What is your intended switching frequency?
Thank you!
0 -
Hello TBhatia,
1. Yes, its soft switching.
2. We are planning to use switching frequency of 5-10HzAlso can i get the I^2t value of TO247-4 and TO247-3 package MOSFETs , as we are looking for through hole package MOSFETs
Regards,
Meghana0 -
Hello Meghana,
We don't have I^2t value for SiC MOSFETs. You can refer to the SOA curve in datasheets for current capacity
Thank you
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0