Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

RC Snubber Design

Maideen
Maideen Contributor Level 1
edited September 2025 in Module Products

For this wplf speed power module (CAB6R0A23GM4T) we have calculated snubber calculation in this way. Could you please verify is it correct. If not, please suggest the right way?
Our ringging frq is 20MHz
Csn=Ls*Ipk^2/Vsn^2 = 30n*180^2/1800^2 = 300pf
Rsn= Sqrt(Ls/Csn)= Sqrt(30n/300p)=10 Ohm
Psn=Csn*Vsn^2*fsw=300p*1800^2*25k=24.3W

jdavidde40

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • CFlack
    CFlack Wolfspeed Employee - Contributor Level 2

    Maideen,

    These calculations make sense from a theoretical perspective. In practice, a capacitor several times larger than the output capacitance is typically required. You may find this article to be of use: Power Tips: Calculate an R-C snubber in seven steps.

    I would suggest initially simulating your design using our LTspice models. As the design progresses, you may choose to evaluate your design in the lab with our 2300 V WolfPACK™ GM SiC Modules Evaluation Kit, which includes pads for device RC snubbers and a DC bus snubber.

    Please let us know if you have further questions. Thanks!

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.