Press-fit pins
There are press-fit pins in 6 pack SiC block.
What exact product to connect those pins to wire or PCB?
Is 5050462-2 will work for that?
If yes, how I solder it to PCB or wire?
In any part of receptacle pin? In front? In back?
Do you have some picture of design?
Comments
-
Hi Pcholka,
I recommend that you reference our WolfPACK module family mounting guide here:
https://assets.wolfspeed.com/uploads/2021/11/cpwr_an41_fm3_mounting_application_note.pdf
This module is intended to be pressed into a PCB directly without any socket or soldering required. This ensures low contact resistance between the pins and the board and is quick & simple to assemble in mass production. If you'd like to use a socket, we recommend the Stäubli BS-1 41.6019 or a Mill-Max 9359 receptacle. A socket is not recommended for use in the end application, but it can be a helpful tool during module validation or test fixturing.
For reference on how the socket can be implemented please see the Dynamic Characterization Evaluation Kit for this module here:
https://assets.wolfspeed.com/uploads/2021/05/cpwr_an44_fmc_application_note.pdf
Best Regards,
Austin C.
0 -
Austin, thank you very much!
That is a complete help.
😀
0