Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CAB600M33LM3 voltage spike on the high side gate after reverse recovery

Options
ralphdeguzman
ralphdeguzman Contributor Level 1

I am working on a double pulse measurements for SiC module CAB600M33LM3 module. I used Rg,off=1.5ohm and Rg,on=2.5ohm and my setup stray inductance is around 12nH. During reverse recovery of the high side diode (Applying double pulse at low side gate), I observe a voltage spike at the high side gate of around 5V peak. This is not observed when I check the reverse recovery of the low side diode. Please see waveform and help to analyze if this is normal or what to do to eliminate such voltage spike. I dont want to risk going into higher drain current because of the possibility of short circuiting the module when this spike really caused the high side switch to turn-on.

Channel 2: High side Vgs

Channel 3: High side Vds

Channel F1: High side Drain Current

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ARK
    ARK Wolfspeed Employee - Contributor Level 1
    Options

    Hello Ralph

    Please share your company email ID and we can reach out to discuss your observations in more detail and provide the solution.

Sign In or Register to comment.