Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Gate Driver Board

Options
Stephen
Stephen Contributor Level 2
edited May 18 in Module Products

May I ask if you have a gate driver board corresponding to the CHB011M12GM4 T-TYPE power module? If you do, could you provide the name?

thanks

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5
    Options

    Hi Stephen,

    We recommend using two of the CGD1700HB2M-UNA-R1 gate drivers. Both channels are isolated with a dedicated DC/DC converter and a Texas Instruments 27710 gate driver IC. These are the same gate drivers that are used for internal Wolfspeed testing. We also have several partner gate drivers in the same footprint and pinout, so the gate drivers can be easily swapped to evaluate performance with different gate driver ICs.

    Thanks,

    Chris N.

    Stephen
  • Stephen
    Stephen Contributor Level 2
    Options

    I understand. I will try using the CGD1700HB2M-UNA-R1 as my gate driver.

    Thanks!

  • Stephen
    Stephen Contributor Level 2
    Options

    Hi ChrisN

    I have another question. If possible, could you provide the PCB files for the CGD1700HB2M-UNA-R1? I didn't see the corresponding resources on the official website.

    Thanks

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5
    Options

    Hi Stephen,

    The design files for the CGD1700HB2M-UNA-R1 are the same as the generic CGD1700HB2M-UNA. The boards share the same schematic and layout, and the design files can be downloaded from the Tools & Support section of the landing page. The only difference is which components are populated on the board to create different output voltages/regulation. These differences are detailed in Section of 4.3 of the CGD1700HB2M-UNA family user guide found here.

    Thanks,

    Chris N.

  • Stephen
    Stephen Contributor Level 2
    Options

    Hi ChrisN

    Do you have PCB files that can be opened with Altium Designer?

    Thanks!

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5
    Options

    Hello Stephen,

    I've attached the STEP file and the converted Altium design files for the CGD1700HB2M-UNA gate driver.

    Thanks,

    Chris N.

  • Stephen
    Stephen Contributor Level 2
    Options

    Hi ChrisN

    THANKS!!!

This discussion has been closed.