Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

XM3 Inverter CAN Interface GUI source code

daveH
daveH Contributor Level 1
edited July 13 in Module Products

HI,

I am currently developing custom control software for a XM3 inverter using the CAN interface.

I am able to run the example code in combination with the supplied GUI. As I develop my controller the I/Os required are different from those in the example so I need to create my own PC software for this, is the python code for CAN interface PC software available anywhere? - as I suspect it would be easier to use this as a starting point rather than having to start from scratch with this

Thanks

Dave

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5

    Hello Dave,

    I sent additional information about the source code to the email address linked to your account. I hope the provided files help you to develop your custom solution. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Thanks,

    Chris N.

This discussion has been closed.