Short Circuit Withstand Capability of Gen. 4 SiC MOSFETs
mathis_picot
Contributor Level 1
Hello,
In your white paper 'Gen 4 SiC Technology: Redefining Performance…', it is stated that the Gen 4 devices can exhibit a short circuit withstand time of up to 2.3 µs.
Could you provide more details on this subject? Such as test parameters, part numbers, waveforms? Any info regarding E4MS025120J2 specifically?
Thank you in advance,
Best regards
0
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Greetings:
Below is a circuit diagram of the short circuit test setup. There also is a screen capture with short circuit waveforms from a C4MS025120K. This part uses the same Mosfet die as the one you are interested in except it is in a 4 lead TO-247 package versus a 7-lead TO-263 package.
Julius R
0