Water leaks spraying modules
Greetings
I designed an LLC resonant inverter who's output will be 125kW at 20kHz nominal, used in the Industrial Induction Heating market. This will use two CAB530M12BM3 devices, configured as an H-Bridge connected to a parallel resonant tank ultimately. We have yet to power up our first prototype, and ran into an issue where the gun drilled heatsink was manufactured incorrect, and leaked water all over the SiC devices, totally soaking them. I am hesitant to use them, they have not had power applied to them yet. The question is, will they still be usable, or are they compromised? Is there a way to save the two devices?
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello LLCInduction,
Thank you for your question and for contacting the Wolfspeed Power Applications Forum.
The ability of the modules to operate safely and reliably after water exposure depends on both the extent of the exposure and the duration of time the modules were in contact with water. Because these modules are not designed with a sealed enclosure, there is a possibility that water may have entered the device.
As a result, Wolfspeed cannot verify or guarantee the functionality, performance, or long-term reliability of the affected modules. If you choose to evaluate or operate the modules, we recommend exercising extreme caution and following all appropriate safety procedures.
For additional information regarding environmental conditions and the reliability of power devices, please refer to the following application note: PRD-06379: Environmental Considerations for Power Electronics.
Please let us know if you have any additional questions. We're happy to help.
Best,
Chad F.
0