Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

10kV SiC driver circuit

daviddavid
daviddavid Contributor Level 1
edited October 23 in Discrete Products

How to drive 10kV SiC mosfet ?

CPM3-10000-0300A


What gate driver and isolated supply is rated for 10kV?

or what custom driver circuit to handle 10kV switching?

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • PaulKanatzar
    PaulKanatzar Wolfspeed Employee - Contributor Level 2

    Hey David,

    A great place to get started with designing a gate driver for the CPM3-10000-0300A is our application note (here) on the best practices for SiC gate drivers. One approach for handling the isolation is to use an off the shelf power supply such as the ISO5125I-120 that is rated for 18 kVrms as the primary power supply for the gate driver. With the main isolation handled, you can implement a gate driver following best practices.

    -Paul

This discussion has been closed.