Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Thermal distribution in CAB006A12GM3T

DNE
DNE Contributor Level 1

Hi,

In our project we use modules CAB006A12GM3T, but now one of them is damaged.

I checked the user guide PRD-07933, Figure.3 on page.4.
The thermal resistance depends mostly by used TIM (60%) and then by DBC (30%).

TIM is pre-applied.
Heatsink is aluminium, liquid cooled.
We use external mixing system with target for input temperature of cooling liquid set at 30 C.

I searching for equation that represents the relation between internal NTC temperature and actual junction temperature.

Best regards
Damyan

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

Sign In or Register to comment.