Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Error in LTspice model for the C3M0030170D

Stephen867
Stephen867 Contributor Level 1

It appears the zero gate voltage drain voltage for this model is incorrect in the sim. With 1000Vds, the drain current was about 11mA. The datasheet says it should be 50uA max at 1700Vds and the sim for that measured 19.4mA

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • BlakeNelson
    BlakeNelson Wolfspeed Employee - Contributor Level 3

    Hi Stephen,

    Unfortunately, the C3M0030170D SPICE model is an older model which does not match the leakage spec and should not be trusted for that parameter.

    I do not have a timeline I can offer you for when it will be updated.

    Let me know if you have any other questions,
    Blake

Sign In or Register to comment.