Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Maximum current of KIT-CRD-3DD12P

xenon
xenon Contributor Level 1
edited October 2022 in Discrete Products

Hi,

I replaced the inductor on the board. The new inductor is rated at 150A. What's the maximum current supported by other parts of the board?

Best Regards

Tagged:

Comments

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 3

    The power terminals are rated for 15A. The MOSFETs will be limited based on thermals which will depend on many factors (switching frequency, voltage, current, airflow).

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. If it did, please click on "This question has been answered - Close Discussion" . If you have a follow up question, at a later date, please "Start a New Discussion" 

This discussion has been closed.