Asking for the structure diagram of KIT-CRD-CIL12N-FMA
Hi, Mr. / Ms.
I'm trying to build an inverter with the module CAB016M12FM3 and the driver board CGD1700HB2M-UNA. I think I need a platform to connect the module and the driver board. I have noticed that the platform KIT-CRD-CIL12N-FMA may be a good choice.
I'm asking for the structure diagram of KIT-CRD-CIL12N-FMA, which looks like the picture below. I can't find a structure diagram of KIT-CRD-CIL12N-FMA in its schematic provided by wolfspeed.
In addition, do you think it's feasible to build an inverter with the platform KIT-CRD-CIL12N-FMA? I mean, if I buy three KIT-CRD-CIL12N-FMA platforms, and then connect their input connections(+V) to the positive pole of the power supply, and also connect their input connections(-V) to the negative pole of the power supply, and finally connect their midpoint connections to a three-phase load, will it work?
Please let me know if you have any questions, comments, or issues.
Thanks!
Comments
-
Hello, thank you for your message. A member of our technical team is looking into your questions and we will respond shortly.
0 -
Hi JunMing,
Please refer to the KIT-CRD-CIL12N-FMA user guide here: https://assets.wolfspeed.com/uploads/2021/05/cpwr_an43_fma_application_note.pdf
The dynamic evaluation boards are not designed to operate continuously like in an inverter application. They should be used for clamped-inductive-load, double-pulse testing only.
Best Regards,
Austin C.
0 -
Thank you very much for your help and your patience!
0