Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

forward threshold voltage and on-state slope resistance (diode) on data sheet

Kilian
Kilian Contributor Level 1
edited April 2023 in General

I have a general question about two values on the datasheet, for example the module CAB011M12FM3:

Where can you find the forward threshold voltage (Diode) (at Tvj= 25°C, 150°C) and the on-state slope resistance, forward slope resistance (Diode) (at Tvj = 25°C, 150°C) on the data sheet? What would the values be for the module CAB011M12FM3?

Thank you,

Kilian

Tagged:

Comments

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hello, thank you for your message. A member of our technical team is looking into your questions and we will respond shortly. 

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4

    Hi Kilian,

    If I understand your question correctly, this information is available in the CAB011M12FM3 datasheet: CAB011M12FM3.pdf" rel="nofollow noopener ugc">https://assets.wolfspeed.com/uploads/2021/05/CAB011M12FM3.pdf

    Body Diode Forward Voltage (VSD) is shown in Figure 7.

    Voltage Threshold (VTH) is shown in Figure 10.

    On-state Current vs. Voltage is shown in Figure 1.

    On-state Resistance (RDS-ON) is shown in Figure 2 & Figure 3.

    Best Regards,

    Austin C.

  • Kilian
    Kilian Contributor Level 1

    Hi Austin,

    thank you for your quick response!

    So the forward threshold voltage of the diode is not a value in the datasheet, you have to use figure 7 to determine it, right? Where can one find the resistance values of the diode?

    Also, are SpeedFit analyses based on formulas or experimental data?

    Thank you so much for your help, I appreciate it!

    Kilian

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4

    Hi Kilian,

    Yes, to determine the voltage & current relationship info on the body diode, you will need to use Figure 7. The diode doesn't have a linear relationship between current and voltage like a resistor, so we do not provide a resistance value.

    The SpeedFit analysis is based on measured data from the module's datasheet characterization.

    Best Regards,

    Austin

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.