Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

The current that the body diode can withstand

baiyujing
baiyujing Contributor Level 2
edited March 2023 in General

When high-power modules such as CAB450M12XM3 operate at high currents (such as 400A), their commutation time is very long. For example, the LTSpice model for dual pulse testing provided by your company sets the dead time after the upper tube is turned off to 5 microseconds, so that the 400A current originally flowing on the lower tube can be converted to the upper tube. The figure shows the current curve of the upper tube. In this way, the current borne by the body diode of the upper tube will be a 400A current of 5 microseconds. Can I use it this way? Because there are similar situations in my project, I hope to receive your guidance.

image.png


Tagged:

Comments

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hello, thank you for your message. A member of our technical team is looking into your questions and we will respond shortly. 

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hello baiyujing,

    I see you had closed this discussion. Does that mean the question has been answered at your end? Thank you so much!

  • baiyujing
    baiyujing Contributor Level 2

    Yes, I have solved this problem

This discussion has been closed.