On Speedfit Design Simulator, both warnings occur at the same time. How can it be solved?
Hi everyone,
I have a question about the loss simulator (Speedfit). When i start to simulate CAB450M12XM3 SiC module according to the parameters below, i'm getting a warning that is showned in the picture below with green highlighted. This is about the load inductance. In the picture above at the schematic view side simulator says L must be higher than 0,01mH. At the bottom side simulator says L must be below 0,01. So, it can not be run to extract the power loss solutions. i appreciate anyone who helps me to solve this. Take care.
Parameters
Modulation Algorithm--> Space Vector, DC Link Voltage--> 800VDC
Output Current--> 324Arms Cont., Output Voltage (Ph-Ph)--> 495Vrms
Output Frequency--> 933Hz, Switching Frequency--> 20kHz
Modulation Index--> 0,875, Power Factor--> 0,78, Load Type--> Inductive
Cooling Condition
Cooling Method--> Liquid, Flow Rate--> 10L/min, Tamb/Coolant-->65ºC
Comments
-
Hello, thank you for your message. A member of our technical team is looking into your questions and we will respond shortly.
0 -
Hi,
This is a known issue and is currently something that we're working on addressing. I've tested this simulation and it seems like the assertion that says that inductance cannot be less than 0.01mH is not valid anymore. This is an active work-in-progress at this time but I recommend checking back within the next day or two and you should be able to run this simulation.
Thanks,
Zack
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0