Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

ECB2R1M12YM3L - Cooling Circuit Pressure

Options
Chris
Chris Contributor Level 1

ECB2R1M12YM3L 1200 V SiC Power Module Data Sheet | Wolfspeed

I'm looking to use the ECB2R1M12YM3L 1200V SiC Power Module for a design and have a couple questions on the cooling circuit:

  1. The datasheet lists the maximum pressure of the cooling circuit as 2.5 bar. Is this a proof or burst limit?
  2. If I stay below 2.5bar, can we expect the module to operate without degradation?
  3. If possible, I would like to request test results or the test spec used to arrive at the max pressure conclusion.

Thank you

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

Sign In or Register to comment.