Regarding the issue of maximum gate voltage
Hello Wolfspeed Team,
I noticed that the datasheet of the 1200 V C3M series SiC MOSFETs specifies:
VGS(max) = -8 V / +19 V
and additionally states:
When using MOSFET Body Diode: VGS = -4 V / +19 V
I would appreciate clarification on the following questions:
- In a normal half-bridge application, the body diode conducts during the dead time. If dv/dt-induced crosstalk, common-source inductance, or other parasitic effects cause the instantaneous gate voltage to drop below -4 V (for example, -5 V) during body diode conduction, does this violate the datasheet limitation?
- Why is the allowable negative gate voltage reduced from -8 V to -4 V when the body diode is conducting? Is this related to gate oxide reliability, threshold voltage shift, interface traps, bipolar degradation, or another mechanism?
- I noticed that a similar requirement does not appear in the datasheets of the 1200 V C4M/C4MS series devices. Does this mean that Gen4 devices no longer have this concern, or does the same limitation still apply but is no longer explicitly stated?
Thank you for your support and clarification.
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello,
Please refer to the latest datasheets of C3M products on Wolfspeed portal, the note of
"When using MOSFET Body Diode: VGS = -4 V / +19 V" has already been removed. Initially, that was just a recommendation for practical application, due to lower minus Vgs induces higher Vf of body diode during freewheeling and finally impacts system efficiency. There is no concern about device reliability without that statement.
Thank you
0