Question regarding drain pin usage
Hello,
I am designing a power bridge with the discretes C3M0016120K (TO247-4). I am wondering if there is any drawback on not using the drain pin and only using the pad as drain electrical contact. With my pre-design there is no room for the pin so I would consider cutting it…
Thanks a lot!!
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Greetings:
I have a few questions about your setup.
- Do you need to isolate the package from the heatsink?
- How do you plan to attach the package to the heatsink?
There's no reason why the drain pad couldn't be used as the electrical contact; however, it would make it difficult if not impossible to isolate the package from the heatsink. If you did need isolation between the package and heatsink, I'm not sure how you would make good electrical contact.
Julius R
0 -
Hello Julius, thanks for the response.
I do not need to isolate the package since the idea is to weld the drain pad to a copper plane with insulation beneath it (and to the heatsink)
0 -
This should work. Just pay attention to your isolation and the resulting total thermal impedance from case to ambient.
Julius R
0