Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

"Direct liquid cooling" of power modules

cweig
cweig Contributor Level 1

Rather than mounting a module such as the CBB011M12GM4T on a "cold plate" would it be possible to mount this module on a liquid-cooling device similar to the "Shower power" system promoted by Danfoss Power Semiconductors? The advantage of this approach is that it eliminates the critical thermal juncture between the module baseplate and yet another metallic surface (requiring TMI or similar materials as interface), both with a non-negligible Rth, by having the cooling liquid in direct contact with the module baseplate itself.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • DustinHill92
    DustinHill92 Wolfspeed Employee - Contributor Level 1
    edited August 12

    Hello,

    As you stated, eliminating layers in the thermal stack can help reduce the overall Rth of a system, with TIM often being a large contributor. Your proposal seems plausible and could be an effective way to reduce thermal impedance if enough engineering time is spent on its implementation. Here are some of the tradeoffs I foresee based on my testing experience:

    Plastic Interface: the plastic thermal interface adds a low thermal conductivity layer to the thermal stack where it contacts the module that may significantly contribute to thermal resistance and reliability concerns.

    Turbulence: the design states it utilizes turbulence to improve localized cooling. Turbulence is often avoided in cooling system design because it increases pressure drop.

    Structure: A baseplateless module lacks the mechanical strength of a baseplate and usually relies on the cold plate it is mounted to assist with this structural stability. Without being attached to a cold plate, the module would have weaker performance with reliability tests like Mechancial Shock and Vibe and Thermal Shock.

    Best regards,

    Dustin

Sign In or Register to comment.