Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

C3M0075120K Rev.6 SPICE model fails in OrCAD PSpice 25.1 at e_P8 — is an official PSpice-compatible

GogoalL
GogoalL Contributor Level 1

Hello Wolfspeed Power Applications Team,

I am using the official C3M0075120K.lib Rev.6 model in an academic power-electronics simulation project and am trying to cross-check the model in OrCAD PSpice A/D 25.1 HF050.

The original, unmodified model is successfully parsed and all subcircuits are loaded, but PSpice fails during Device/Model Load before the first Newton iteration (NUMNIT=0) at X_DUT.xgmos.e_P8 / line 177 with ORPSIM-16551 floating-point overflow.

The canonical model file used in our test is 8,336 bytes with SHA-256:

F0FBD41D9F10351756AB6F784340759781B5B294FC22795E4D0131216E53D553

We also tested .NODESET and .OPTIONS LIMIT; neither makes the original expression execute successfully. A diagnostic numerically guarded evaluation can get past the initialization overflow, but we do not want to modify the vendor model without an authoritative compatibility definition.

Could you please clarify:

  1. Is the current Rev.6 C3M0075120K.lib intended to be compatible with OrCAD PSpice?
  2. Is there an official PSpice-compatible version or compatibility patch for C3M0075120K?
  3. If an earlier standalone model revision was PSpice-compatible, could you provide that revision or its revision/date information for comparison?
  4. Are there documented compatibility transformations required for the e_P8 expression, particularly Limit, exponentiation/fractional-power evaluation, or related behavioral-source semantics?

I can provide a minimal .op reproducer and the PSpice error log if useful.

Thank you.

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

    GogoalL
Sign In or Register to comment.