C3M0075120K Rev.6 SPICE model fails in OrCAD PSpice 25.1 at e_P8 — is an official PSpice-compatible
Hello Wolfspeed Power Applications Team,
I am using the official C3M0075120K.lib Rev.6 model in an academic power-electronics simulation project and am trying to cross-check the model in OrCAD PSpice A/D 25.1 HF050.
The original, unmodified model is successfully parsed and all subcircuits are loaded, but PSpice fails during Device/Model Load before the first Newton iteration (NUMNIT=0) at X_DUT.xgmos.e_P8 / line 177 with ORPSIM-16551 floating-point overflow.
The canonical model file used in our test is 8,336 bytes with SHA-256:
F0FBD41D9F10351756AB6F784340759781B5B294FC22795E4D0131216E53D553
We also tested .NODESET and .OPTIONS LIMIT; neither makes the original expression execute successfully. A diagnostic numerically guarded evaluation can get past the initialization overflow, but we do not want to modify the vendor model without an authoritative compatibility definition.
Could you please clarify:
- Is the current Rev.6
C3M0075120K.libintended to be compatible with OrCAD PSpice? - Is there an official PSpice-compatible version or compatibility patch for
C3M0075120K? - If an earlier standalone model revision was PSpice-compatible, could you provide that revision or its revision/date information for comparison?
- Are there documented compatibility transformations required for the
e_P8expression, particularlyLimit, exponentiation/fractional-power evaluation, or related behavioral-source semantics?
I can provide a minimal .op reproducer and the PSpice error log if useful.
Thank you.
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0