Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

What is included in the datasheet Eon/Eoff values?

rlarjsdn
rlarjsdn Contributor Level 1

Hello,

First of all, thank you for your products. I have been using Wolfspeed devices and am currently working on a design with the C3M0060065K.

I have a question about the Eon value specified in the datasheet. Does it represent the total loss, including the body diode reverse recovery loss, Coss loss, dead-time loss, gate charge loss, and so on?

Thank you.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • SudharsanC
    SudharsanC Wolfspeed Employee - Contributor Level 1

    Hello,

    Thank you for using Wolfspeed devices and for your question.

    The Eon value specified in the datasheet represents the turn-on switching energy measured under the specified test conditions in the datasheet.It represents the energy dissipated in the MOSFET during turn-on and the effect of commutating current from the complementary freewheeling device (MOSFET body diode or external SiC Schottky diode) present in the test circuit. As a result, Eon depends on both the MOSFET characteristics and the switching conditions.

    However, Eon does not represent the total converter loss. The following losses must be evaluated separately:

    • Conduction losses (RDS(on)-related)
    • Output capacitance (Coss) losses
    • Dead-time losses
    • Gate-drive losses (Qg × VGS × switching frequency)
    • Body diode conduction losses
    • Other application-specific losses

    Therefore, Eon and Eoff should be used as the switching-loss components measured under the specified test conditions, while the remaining loss mechanisms should be calculated separately to estimate overall converter efficiency.

    Best regards,

    SudharsanC

  • rlarjsdn
    rlarjsdn Contributor Level 1

    Thank you for the detailed answer!

    It was very helpful.

Sign In or Register to comment.