What is included in the datasheet Eon/Eoff values?
Hello,
First of all, thank you for your products. I have been using Wolfspeed devices and am currently working on a design with the C3M0060065K.
I have a question about the Eon value specified in the datasheet. Does it represent the total loss, including the body diode reverse recovery loss, Coss loss, dead-time loss, gate charge loss, and so on?
Thank you.
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello,
Thank you for using Wolfspeed devices and for your question.
The Eon value specified in the datasheet represents the turn-on switching energy measured under the specified test conditions in the datasheet.It represents the energy dissipated in the MOSFET during turn-on and the effect of commutating current from the complementary freewheeling device (MOSFET body diode or external SiC Schottky diode) present in the test circuit. As a result, Eon depends on both the MOSFET characteristics and the switching conditions.
However, Eon does not represent the total converter loss. The following losses must be evaluated separately:
- Conduction losses (RDS(on)-related)
- Output capacitance (Coss) losses
- Dead-time losses
- Gate-drive losses (Qg × VGS × switching frequency)
- Body diode conduction losses
- Other application-specific losses
Therefore, Eon and Eoff should be used as the switching-loss components measured under the specified test conditions, while the remaining loss mechanisms should be calculated separately to estimate overall converter efficiency.
Best regards,
SudharsanC
0 -
Thank you for the detailed answer!
It was very helpful.
0