SPEEDVAL KIT HALF-BRIDGE MOTHERB : MOD-MB-HB-0900V-40A Single phase inverter testing
Dear all,
I have question about SPEEDVAL KIT HALF-BRIDGE MOTHERB : MOD-MB-HB-0900V-40A.
I'd like test sinlge phase inverter using it.
However, there is no reference about it in the datahseet.
I think it is possible to test single phase using the speedval kit.
I have questions about it.
Question 1) DC link cap
One thing I concered is that DC link cap.
Does it include DC link cap or not? more specific, the DC link cap should be splited by VDC/2.
Question 2) Modify the speed kit
Also, I'd like to modifiy the test kit to auxiliary resaonant commutated pole inverter(ARCP).
Red one is the Speed kit and other things are the external one.
Have you tried like this circuit? I think it is possible. Do you have any concern about the configuration?
Question 3) Dspace.
I'd like to use DSpace as the gate signal function generator.
This is becauase the mother board can suport external fuction generator using BNC cable.
Have you test it using Dspace?
Best regards,